Search found 6 matches

by stephen112
Wed May 15, 2019 2:39 am
Forum: BeagleBone
Topic: BBGW and USB Audio?
Replies: 4
Views: 894

Re: BBGW and USB Audio?

Thanks for your response! After reading a lot and editing the config files (/etc/modprobe.d/alsa-base.conf, /usr/share/alsa/alsa.conf, /etc/asound.conf), I got it working with the c-media usb sound card. The only issue is that for some reason, I have to sudo the alsa commands for them to work. I log...
by stephen112
Fri May 10, 2019 2:07 pm
Forum: BeagleBone
Topic: BBGW and USB Audio?
Replies: 4
Views: 894

Re: BBGW and USB Audio?

To add some more detail, if I try the simplest aplay command, aplay Flute02.wav I get the error message, ALSA lib dlmisc.c:254:(snd1_dlobj_cache_get) Cannot open shared library /usr/lib/arm-linux-gnueabihf/alsa-lib/libasound_module_pcm_front.so aplay: main:788: audio open error: No such device or ad...
by stephen112
Fri May 10, 2019 1:15 pm
Forum: BeagleBone
Topic: BBGW and USB Audio?
Replies: 4
Views: 894

BBGW and USB Audio?

Hello all, I have a new BBGW and have updated it to the latest Debian (4.14.108-ti-r104). I want to do audio I/O using a C-Media sound card. The lsusb command tells me, Bus 001 Device 003: ID 0d8c:0102 C-Media Electronics, Inc. CM106 Like Sound Device and aplay -L appears to find the card's many por...
by stephen112
Fri May 10, 2019 12:59 pm
Forum: BeagleBone
Topic: Where can I get the boot image for the BBGW?
Replies: 4
Views: 769

Re: Where can I get the boot image for the BBGW?

Many Thanks !!
by stephen112
Wed May 08, 2019 1:33 am
Forum: BeagleBone
Topic: Where can I get the boot image for the BBGW?
Replies: 4
Views: 769

Re: Where can I get the boot image for the BBGW?

Thanks for your response, but if I boot the default image,

https://debian.beagleboard.org/images/b ... 07-4gb.img

it doesn't start the WiFi services or the LED-flashing demo.

Is there a source for the actual image that comes pre-installed on the BBGW?

stp
by stephen112
Tue May 07, 2019 8:59 am
Forum: BeagleBone
Topic: Where can I get the boot image for the BBGW?
Replies: 4
Views: 769

Where can I get the boot image for the BBGW?

Hi all, I appear to have bricked my new BBGW (editing the demo script /boot/uEnv.txt as described in the doc, so that it no longer completes the boot process). I don't have a 3.3V serial adapter handy, so I'm trying to get the unit to boot from a USB stick to re-edit the start-up script. Is there a ...