Search found 5 matches

by vega4ref
Tue Oct 22, 2013 4:31 pm
Forum: RePhone
Topic: ArduinoPhone
Replies: 68
Views: 119807

Re: ArduinoPhone

FIXED THE PROBLEM. The necessary library was not TFT_v2/TFT_v2.h but it was SeeedTFTv2/TFTv2.h. http://www.seeedstudio.com/wiki/File:Seeed_TFT_v2.0.zip This TFTv2.h has that same 6 integer input as was used in TFT version 1.0. Now it is displaying what it is supposed to. However the time and date do...
by vega4ref
Tue Oct 22, 2013 4:04 pm
Forum: RePhone
Topic: ArduinoPhone
Replies: 68
Views: 119807

Re: ArduinoPhone

The inputs to fillScreen are different in TFT.h and TFT_v2.h! In TFT.h you have: void fillScreen(unsigned int XL,unsigned int XR,unsigned int YU,unsigned int YD,unsigned int color); this is the format used in UI_ArduinoPhone.cpp. However in TFT_v2.h you have: void fillScreen(unsigned int color); Is ...
by vega4ref
Tue Oct 22, 2013 3:57 pm
Forum: RePhone
Topic: ArduinoPhone
Replies: 68
Views: 119807

Re: ArduinoPhone

Hello vega4ref, as far as I remember I had the white screen as well when I compiles the original Arduino Code with the TFT 2.0. So u need the new libraries. Did you changed in teh code " Tft.TFTinit(); " to " // Tft.init(); " (without the ") ? maybe search for the string Tft.init() all over the cod...
by vega4ref
Mon Oct 21, 2013 11:43 am
Forum: RePhone
Topic: ArduinoPhone
Replies: 68
Views: 119807

Re: ArduinoPhone

Hello, 1) no,this GPRS Shoield is only newer version as far as i read! U need to put an battery inside. do not know why, but without was not working. the battery in the rtc timer keeps the clock working when power is disconnected. 2) no, should make no difference.For testing you need only connect t...
by vega4ref
Sun Aug 11, 2013 10:14 am
Forum: RePhone
Topic: ArduinoPhone
Replies: 68
Views: 119807

Re: ArduinoPhone

Hello, I have purchased the kit with everything, and I need a bit of help connecting each piece as I am newcomer to electronics. What I have are: Arduino Uno GPRS Shield V2.0 TFT V2.0 Grove RTC Li Po Rider Pro and battery My questions are following: 1) The GPRS shield I bought looks different than t...