Search found 7 matches

by desmondandrewcorreia
Fri May 24, 2013 12:31 am
Forum: Bee series & WSN
Topic: BlueTooth Bee AT command set
Replies: 9
Views: 6192

Re: BlueTooth Bee AT command set

I still don't see why I have to buy it that would be a waste of money if you ask me. I have both an ARM processor and Amtel micro that can talk to the flash memory via UART. So it's either the firmware that on it is just not very good or the BC417 is damaged. Anyway I already built my self the progr...
by desmondandrewcorreia
Thu May 23, 2013 2:51 pm
Forum: Bee series & WSN
Topic: BlueTooth Bee AT command set
Replies: 9
Views: 6192

Re: BlueTooth Bee AT command set

Why would I need the bluetooth bee standalone. How does this help me I already have an ardunio and I can communicate with the flash memory, I just don't think it's correctly setting up the BC417, but the flash memory is just responding. I will check the wiring to see where the LED connect to and wha...
by desmondandrewcorreia
Thu May 23, 2013 12:24 pm
Forum: Bee series & WSN
Topic: BlueTooth Bee AT command set
Replies: 9
Views: 6192

Re: BlueTooth Bee AT command set

I have already tried that, and if i save the pincode once it shouldn't have to be set again. That would make no sense to me. Why would i have to set the pincode on the device after every reboot?
by desmondandrewcorreia
Thu May 23, 2013 3:25 am
Forum: Bee series & WSN
Topic: BlueTooth Bee AT command set
Replies: 9
Views: 6192

Re: BlueTooth Bee AT command set

I having some trouble. Not matter what mode I put the blue tooth bee in, I can't seem to find it using my android phone or my computer. The bluetooth bee needs to be in Slave mode to connect to my computer/phone and I have done this. Here is the response from the module. Setting up Bluetooth link +S...
by desmondandrewcorreia
Wed May 22, 2013 4:47 pm
Forum: Bee series & WSN
Topic: Set up connections between two BluetoothBee step by step
Replies: 38
Views: 91610

Re: Set up connections between two BluetoothBee step by step

I having some trouble. Not matter what mode I put the blue tooth bee in, I can't seem to find it using my android phone or my computer. The bluetooth bee needs to be in Slave mode to connect to my computer is that correct? Here is the response from the module. Setting up Bluetooth link +STWMOD=0 OK ...
by desmondandrewcorreia
Wed May 22, 2013 3:37 am
Forum: Bee series & WSN
Topic: BlueTooth Bee AT command set
Replies: 9
Views: 6192

Re: BlueTooth Bee AT command set

I already read that post. It's not helpful to me. I want to know the firmware version. Because I am guessing it's firmware HC06. I want to use HC05, since it supports I/O pins. I didn't feel like reading the entire datasheet on the flash memory to figure out how to program the flash memory, I was ho...
by desmondandrewcorreia
Tue May 21, 2013 8:42 am
Forum: Bee series & WSN
Topic: BlueTooth Bee AT command set
Replies: 9
Views: 6192

BlueTooth Bee AT command set

Hello, I bought a bluetooth bee a while back. I am wondering how I could figure out what firmware it run. Also where could I find the command set for this bluetooth bee. The data on it is 12/02/2009. The bluetooth bee really doesn't have any other usefull information. Written on it. I want to be abl...