Search found 20 matches

by byronjbignell
Fri Aug 31, 2018 6:43 am
Forum: Arduino & Seeeduino
Topic: Arduino Mini as Slave to Linkit One as Master
Replies: 0
Views: 528

Arduino Mini as Slave to Linkit One as Master

Hello, I've rigged up an arduino mini-pro as a slave to a linkit one; I needed more interrupts for the data logger I've been building. I've got the slave sending anemometer data to the master via wire() & I2C, the problem I'm having is that only some of the data is getting sent. I've attempted loopi...
by byronjbignell
Sat Mar 14, 2015 1:17 am
Forum: Arduino & Seeeduino
Topic: Connecting 2 Grove devices to Stalker 3.0
Replies: 11
Views: 5978

Re: Connecting 2 Grove devices to Stalker 3.0

You're right, the temp is always better from an external device since the case is waterproof. I use external DHT-11/22 sensors for that reason.

The new files (in the .rar file in Jacket's reply) solve the issue with the DHT devices.

B
by byronjbignell
Tue Mar 03, 2015 9:59 am
Forum: Bee series & WSN
Topic: +BTSTA:xx
Replies: 1
Views: 1274

Re: +BTSTA:xx

It really just appears that there's no way to actually interrogate the BT Bee and get a real status / state from it - at least not from the Stalker base shield - in this case. I really wish there were a more capable base shield like the stalker that provided the same utility but with better support ...
by byronjbignell
Tue Mar 03, 2015 1:35 am
Forum: Bee series & WSN
Topic: +BTSTA:xx
Replies: 1
Views: 1274

+BTSTA:xx

I'm trying to control the on-off state of the Bluetooth Bee I'm using. I've tied it to the state of the solar panel by getting the charge state - basically, if the panel is charging it's daylight so turn the Bluetooth Bee 'on' and configure to be inquirable - which means that if the charge state is ...
by byronjbignell
Mon Mar 02, 2015 9:55 am
Forum: Bee series & WSN
Topic: Stalker 3 and 2.3 + BT Bee - solution
Replies: 0
Views: 1221

Stalker 3 and 2.3 + BT Bee - solution

So here's a solution, and code for anyone dragging themselves through the muck trying to get a seeeduino stalker 3 (or 2.3) to run with a bluetooth bee. A couple of things. One, it's still a little slow. Two, there's probably a solution to that, I just haven't found it yet. The sketch below will con...
by byronjbignell
Mon Mar 02, 2015 9:54 am
Forum: Bee series & WSN
Topic: Bluetooth bee pairs and then drops pairing
Replies: 2
Views: 2039

Re: Bluetooth bee pairs and then drops pairing

A solution, and code for anyone dragging themselves through the muck trying to get a seeeduino stalker 3 (or 2.3) to run with a bluetooth bee. A couple of things. One, it's still a little slow. Two, there's probably a solution to that, I just haven't found it yet. The sketch below will connect you, ...
by byronjbignell
Sat Feb 28, 2015 11:35 pm
Forum: Bee series & WSN
Topic: Bluetooth bee pairs and then drops pairing
Replies: 2
Views: 2039

Re: Bluetooth bee pairs and then drops pairing

It turns out the problem is a little more complex than first noted. The BT Bee can (and is) made "inquirable" and can be paired with a laptop / android device, though it is having issues pairing with a mac laptop; it did pair successfully a few times during testing to the macbook I use but has not b...
by byronjbignell
Sat Feb 28, 2015 9:29 am
Forum: Bee series & WSN
Topic: Bluetooth bee pairs and then drops pairing
Replies: 2
Views: 2039

Bluetooth bee pairs and then drops pairing

Hi,

Any ideas why a bluetooth bee will successfully become inquirable but then fail (go nin-inquirable) when attempting to pair a laptop or an android device with it?

Solved. See comment below:

B
by byronjbignell
Sat Feb 28, 2015 12:39 am
Forum: Bee series & WSN
Topic: Elecrow HC-5 Bluetooth bee / Stalker 2.3 & 3
Replies: 2
Views: 1949

Re: Elecrow HC-5 Bluetooth bee / Stalker 2.3 & 3

As it happens - as confirmed by the folks as Seeed Studio there is a defect in the Stalker 3 board that prevents Bee devices from working on software serial - so, that's fun. It means you can (and have to) use the hardware serial pins to communicate with the bee device, in this case a bluetooth bee....
by byronjbignell
Fri Feb 27, 2015 11:50 pm
Forum: Arduino & Seeeduino
Topic: Stalker 2.3 & 3 and elecrow HC-5 bluetooth bee 2.0
Replies: 4
Views: 2828

Re: Stalker 2.3 & 3 and elecrow HC-5 bluetooth bee 2.0

Hi, So I found a defect in the design of the Stalker 3 board. So, what's the prize for that? I have got the Stalker 3 working with a Bluetooth Bee now using the hardware serial, next is to configure the reading of the data from the SD card and then stream it to the master (a computer or Android phon...