Search found 4 matches

by cb719
Thu Jun 13, 2019 11:10 pm
Forum: ReSpeaker
Topic: Respeaker USB: Holes position?
Replies: 4
Views: 1182

Re: Respeaker USB: Holes position?

Thank you very much!
by cb719
Sat May 18, 2019 8:28 pm
Forum: ReSpeaker
Topic: Respeaker USB: Holes position?
Replies: 4
Views: 1182

Re: Respeaker USB: Holes position?

I'm referring to the Respeaker USB 4 Mic Array:
https://respeaker.io/usb_4_mic_array/

A schematic with the exact position of the 3 mounting holes would be nice to have.
by cb719
Fri May 03, 2019 5:05 am
Forum: ReSpeaker
Topic: Respeaker USB: Holes position?
Replies: 4
Views: 1182

Respeaker USB: Holes position?

Hi there,

Does anyone have a blueprint/drawing showing the position of the 3 holes on the respeaker USB?
I'd like to make a cover but it's a difficult to measure.

Thanks :)
by cb719
Sun Apr 28, 2019 1:35 am
Forum: ReSpeaker
Topic: USB 4 Mic Array: Connect via Pins instead of USB?
Replies: 1
Views: 515

USB 4 Mic Array: Connect via Pins instead of USB?

Hi there, I have two question regarding the Respeaker USB 4 Mic Array: 1. Is it possible to connect USB via the pins on the bottom instead of the Micro USB connector? I want to save space at the side. 2. Does it have an amplified output on the bottom pins so I can connect a non-powered speaker? E.g....