Search found 3 matches

by alina06
Wed Apr 24, 2019 3:41 am
Forum: Grove
Topic: 128x128 oled
Replies: 9
Views: 2489

Re: 128x128 oled

I have several oled displays 128x32, 128x64, both spi and i2c versions. I bought the grove 128x128, and I can run the seeedgrayoled arduino sketch and see 12 lines of hello world in the 96 by 96 box, but thats not a very good example. FileZilla UC Browser Rufus It should at least be able to draw li...
by alina06
Wed Apr 24, 2019 3:25 am
Forum: Grove
Topic: Tutorial: Reading Water Flow rate with Water Flow Sensor
Replies: 34
Views: 180476

Re: Tutorial: Reading Water Flow rate with Water Flow Sensor

eltoddo: Yes, it will be off 1.5cl in the worst case. If, and only if, the accuracy is constant for a certain device, it can be configured. Lets say you have constant -1% error in measured vs. real value, (aka. 50cl measured, 50.5cl real) you pull 1.01 as multiplier into the code. In +1%, you use 0...
by alina06
Tue Apr 16, 2019 7:09 pm
Forum: Arduino & Seeeduino
Topic: Atom Node (beaconui Android version)
Replies: 4
Views: 5092

Re: Atom Node (beaconui Android version)

In case anyone else who has an Atom Node that wants to try out the BeaconUI Android app (a working version) I finally found one here: https://github.com/yexiaobo-seeedstudio/BeaconUI the .apk is in the /bin directory I tested it and works fine on a Samsung Galaxy S6 running Android 7.0 Now, the nex...