Search found 2 matches
- Sun Apr 21, 2019 11:10 am
- Forum: Hardware Products for AIoT Applications
- Topic: MAix GO/Dock/BiT Project Source Files
- Replies: 3
- Views: 1874
Re: MAix GO/Dock/BiT Project Source Files
OK so how about a differnt request? I want make a carrier board to mount the DOCK PCB so I can access all I/O in a prototype application but I can't find an accurate diagram for the drill hole patterns. Some dimension are shown in "Sipeed Maix-GO Specifications_EN V1.0.pdf" they are only for the ove...
- Fri Mar 29, 2019 4:27 pm
- Forum: Hardware Products for AIoT Applications
- Topic: MAix GO/Dock/BiT Project Source Files
- Replies: 3
- Views: 1874
MAix GO/Dock/BiT Project Source Files
I've been wondering if the schematic/PCB source file format for these boards is known and available for use as a starting point for custom projects. I know that the PDF's are available but why reinvent the wheel (board)?