Search found 350 matches

by loovee
Tue Feb 23, 2016 9:46 am
Forum: Shields
Topic: CAN-BUS Shield V1.2 - can-bus baud rate vs serial baud rate?
Replies: 1
Views: 1631

Re: CAN-BUS Shield V1.2 - can-bus baud rate vs serial baud r

Hi, I'm connecting to a CAN-BUS with 100Kbps. What should my baud rate be set for my Serial? is 9600 sufficient or I should use higher 115200 (since 100Kbps is 100000bps)? Or would that depend on how much and how often data is send on CAN-BUS? I'm using the shield to receive (with mask and filter) ...
by loovee
Sun Feb 14, 2016 2:22 pm
Forum: RePhone
Topic: CDMA version of RePhone
Replies: 1
Views: 1549

Re: CDMA version of RePhone

Are the design engineers considering a CDMA version of RePhone? Verizon and Sprint are CDMA based carriers, not GSM. Would be great to have a CDMA version of the RePhone. Any updates here? Hi, 4G version is on developing already, but it's still too early to talk about when it will come out. Thanks.
by loovee
Sun Feb 14, 2016 2:17 pm
Forum: RePhone
Topic: Is the Rephone kit manual online somewhere?
Replies: 1
Views: 1376

Re: Is the Rephone kit manual online somewhere?

seeedstudio201407 wrote:Hello:

Is the Rephone kit manual online somewhere? The kit comes with a physical manual that is VERY useful.

I guess I could scan it but :
1) Where would I post it?
2) Would it be violating copyright if I did?

Charlie in Houston
Hi, please feel free to post it to ANYWHERE.
Thanks.
by loovee
Sun Feb 14, 2016 2:14 pm
Forum: Shields
Topic: CAN-BUS Shield V1.2 - Power switch function
Replies: 1
Views: 2459

Re: CAN-BUS Shield V1.2 - Power switch function

Hi to all, on the shield there is a power switch: how does it works? When I switich on and off, the shield continue to work regulary, I cannot appreciate diferences between ON and OFF... :o I'm using the conneiction from the CAN terminal (green connector with 2 screws), could you clarify the functi...
by loovee
Sun Feb 14, 2016 2:10 pm
Forum: Shields
Topic: CAN Bus shield 1.2 not receiving messages from vehicle CAN
Replies: 6
Views: 6691

Re: CAN Bus shield 1.2 not receiving messages from vehicle C

Hello, sorry for the delay reply, just come back to office for the Chinese New Year.
I have some questions for more details.

1. Do you know the baudrate of you vehicle exactly? Maybe the baudrate is not include in the library.
2. Does the led_int blink?

Thanks.
by loovee
Sun Feb 14, 2016 2:03 pm
Forum: Shields
Topic: CAN-BUS Shield V1.2 and OBDII Library
Replies: 2
Views: 3420

Re: CAN-BUS Shield V1.2 and OBDII Library

Hi, I am sorry there's no obd library, but a simple demo, please refer to https://github.com/Seeed-Studio/CANBUS_ ... BD_RECIPLE

Thanks.
by loovee
Sun Feb 14, 2016 1:59 pm
Forum: LinkIt
Topic: 3D sketch for the arduino breakout
Replies: 2
Views: 3651

Re: 3D sketch for the arduino breakout

LinkIt ONE?
What kind of format do you need?
by loovee
Thu Jan 28, 2016 3:33 pm
Forum: Arduino & Seeeduino
Topic: 2.8 Touch TFT GUI button help
Replies: 1
Views: 2095

Re: 2.8 Touch TFT GUI button help

There's a bmp display examples in the library.
Please have a try, thanks.
by loovee
Tue Jan 26, 2016 4:16 pm
Forum: RePhone
Topic: Main Button
Replies: 1
Views: 1868

Re: Main Button

Hi, the button can be act as normal button.
please refer to ..\\Eclipse 2.0.46\LINKIT_ASSIST_SDK\examples\API\Framework_Keypad

But long press to turn off can't be change, it's set in the firmware.
Thanks.
by loovee
Tue Jan 26, 2016 4:14 pm
Forum: RePhone
Topic: (TECH)arduinoprogram demolition
Replies: 3
Views: 1474

Re: (TECH)arduinoprogram demolition

Hi, I have tested for 30 mins and don't find any wrong.
Is there any change in your code? and what's the firmware version of your board?
Thanks.