For me it says that file was written sucesfully, but it is not readable for me either. I can see it on quad disk, see the filename, filesize, but canāt read/copy it.
Same here. The UI reports āsuccesfully writtenā for both file types - but I have the same symptoms described above.
Now I can read the files with DiskGenuis file restorer application.
Sounds like there might be some issue updating the filetable here for some reason then ?
Hi,
New version is up on the site:
http://essentialscrap.com/dsoquad/LOGICAPP.HEX
Apparently Windows, usually so ignorant of filename case-sensitivity, refuses to read lower-case filenames from a FAT12 partition. I guess it is correct behaviour per the spec, but didnāt notice the problem as the lower-case files worked fine on Linux.
thanks jpa works like a charm now
Found a ābugā, but its really only present during dumb user interaction
If you hit āsave fileā while its still filling the buffer, it will start saving the file blocking until the buffer reaches 100%. It then reports written succesfully, but if you then press ābmpā it starts saving, then crashes and produces a streaky LCDā¦
Not really an operational issue - but maybe it might be worth making it stop filling the buffer if the user hits āsave fileā ?
Hmm, I canāt repeat your issue. Both BMP and VCD save fine even when the capture is still running. When did you buy your DSO Quad (maybe it is the processor revision issue again)?
It should be perfectly capable of capturing data while saving at the same time. But saving the VCD takes a long time because the write speed to the USB disc is only 25kB/s.
Hmmā¦ I was able to reproduce it pretty consistently last night but today it doesnāt play ball.
Let me keep investigating.
And I bought mine via a Seeed reseller in January, however it might be as old as August 2011 stock though. Hard to tell really I guess. Do the serial numbers correlate in anyway ?
Iām trying to analyze two serial streams that I have captured. I would like to view them side by side, one with a known good command and another with a command that is being questioned. I got good data into the DSO QUAD, and have two separate VCD files. I have them open in GTKWave, but am now having some troubles analyzing them. This could just be learning curve, but I think itās more than that at this point.
Fist problem Iām having, when I choose hex display, it doesnāt seem to react. Even if it did, I would expect the sample rate is not correct. 2uS is way off from the 9600 Iām working with.
Second problem, I canāt display traces side by side. If I could simply place the two traces side by side I could look at them and see what bits are different. However no dice, I have to switch from tab to tab to see if I can notice a difference.
Any thoughts? Sorry I donāt know how to get an attachment to stick I would post the files for folks to review.
Iām using GTKWave 3.3.8 on Win7 64 bit. Iāll try this again when I have access to a Ubuntu 64 bit machine.
GTKWave does not have any UART decoding, so hex display means that if you have multi-bit signal it shows it as hexadecimal. If you only have 1 bit signal, hex display of 1 is still just 1
2ĀµS is the internal sample rateā¦ I expect that the pulses in your serial signal should be multiple samples long, so if you measure times in gtkwave they should be correct.
To display multiple wave files side-by-side, easiest is probably to open multiple instances of gtkwave and resize the windows. Other option is to use some tool that can join 2 VCD files to 1 VCD file.
The combine up and combine down thing in GTKWave seems to do something, but like the help file notes, itās next to useless on one signal. Even if I had two signals, I donāt quite know what to expect. I got over the issue I was working with, by using the DSO to check signal integrity, then connected with putty to decode hex values. With the DSO I was able to verify there werenāt any reflections causing an odd bit, or anything like that.
Are there any programs that can extract a serial UART stream out of a VCD file? It would have been real handy for the problem I was working on. I have found some purchased products that appear to do it, however I havenāt had luck yet finding one for a vcd file.
Also this logic analyzer application is great. Thanks for creating that. Much appreciated.
Yeah. I wonder if the software for Open Logic Sniffer has some UART decoding. I might add support for its format at some time.
I hope to add built-in UART, SPI, I2C, USB etc. decoding at some time in the future, but it may be a while before I have the time to do that. The groundwork is laid, but I have some performance problems in the signal decoding (it needs to decompress and seek the signal dozens of times, I need to add some kind of a cache).
It does.
Dear jpa.
In what there can be a problem?
At me one and the same LOGICAPP version (last) isnāt always started after installation. It is necessary rewrite several times.
Any error message? Do you get an infinite ābeeeeeeeeeeeepā?
Just restarting it many times is not enough, i.e. it is a problem in flashing?
Maybe you have a bad USB cable for the installation or something.
Isnāt present it isnāt a cable. Old the version (66,3 kb) is steadily started after installation. New version (10.01.13) very seldom is established correctly and then it is started work. Each time different figures last line STACK DUMP.
Thanks for the photo. It helps a lot.
Just reminders to myself:
- PC is totally crazy, so it has jumped to some random place
- LR is in add_malloc_block, on the line calling malloc_lock() using āblx r3ā
- R3 agrees with the incorrect PC value after the jump
- malloc_lock is a function pointer in static variable
- Somehow the initialization of the .data section must have failed
- Turns out GCC 4.7.3 LTO bugs were again bothering me. I already disabled it in QuadPawn, now it is disabled in Logic also.
The reason I hadnāt noticed is that I apparently had an old version installed on my own device for some reason.
Now there is 0.2 uploaded, it should work:
http://koti.kapsi.fi/~jpa/dsoquad/#Logic%20Analyzer
LOGIC02 began to be started normally, but when pressing the SAVE button jumps out the red screen.
P.S. What is the settings? How to use them?
Ah bah, bug fixed in 0.3.
The settings menu is work-in-progress. Currently you can just enable snap-to-edges there.
I havenāt had much time to work on this app lately, but itās good that someone tests that it still works
Excellent work. The main functions work as it is necessary. There is a small problem with memory dump. If to make a choice of this point, there is a red screen. The memorydmp file is created. This file canāt be removed from a flash card (there is no access) or canāt be read, only a disk format.