Randomly pausing only through respeaker bluetooth

I’m testing the ReSpeaker as a Bluetooth Player-Master Device. The source is an Android mobile (OnePlus), and it is paired to Respeaker via Bluetooth. Unfortunately the ReSpeaker pauses at random intervals multiple times throughout every song I play.



I’m recording the situation with other mobile, and you will hear the pauses if you play the mp3 file:
[attachment=2]respeaker_record.mp3.zip[/attachment]

It doesn’t happen when I play it directly through my phone nor my BT headphones. It means that the reason of the problem is not source, it can be excluded.



The top program provides a dynamic real-time view of a running system, as I see, there is not any process which affects to performance or there is any performance issue:
[attachment=1]20180602_193528.png[/attachment]

Is anyone else experiencing the same issue?



I’m using Android 8.1:
[attachment=0]Screenshot_20180602-201018.jpg[/attachment]
Screenshot_20180602-201018.jpg
20180602_193528.png
respeaker_record.mp3.zip (1.38 MB)

Hi there:

First you can usred command "kill -9 " to killed usr/bin/pulseaudio --start --log-target=syslog processed.and then play the music.

Hi, I killed pulseaudio task and the music was disappeared. maybe pulseaudio is needed to playing music.

I don’t know.



Any idea?

Dear Customer,

It is a known bug, the software engineers work on the solutions now. thanks.

Seeed tech support team

Bill