Hi there, please help me about Bluetooth issue.
Today the device is arrived, based on your instruction wifi is configured well, but the Bluetooth is not working.
Here is the commands:
[attachment=2]20180517_214403.png[/attachment]
Of course at the end there was
command.
And now the device is not available on my Android:
[attachment=0]20180517-215514.png[/attachment]
Thank you in advanced!
ITC
there is something wrong:
[attachment=0]20180517_220216.png[/attachment]
Hi there:
cd /lib/systemd/system/
Find the file “brcm.service”,Change the inside bcm43438a0.hcd to bcm43438a1.hcd,And then reboot
This is a current Firmware bug. This will be fixed in the next firmware update.
Thank you, connection is OK I can connect to “Respeaker-20C7” device.
Can I use Respeaker as a Bluetooth speaker. I would say, “Respeaker, Bluetooth” or “Respeaker, pair,” to begin pairing? - after the first pairing the Respeaker knows my device and can run the music player on Android and can play music, what I want it.
Hi there:
Your idea is very good, theoretically can be achieved, but the code yourself to complete.