Wio Link Frequently Asked Questions (FAQ)

Simplify IoT Development.

Moderators: violet, yexiaobo, seth.welday

Post Reply
yexiaobo
Pre-kindergarten
Pre-kindergarten
Posts: 46
Joined: Tue Dec 11, 2012 10:53 am

Wio Link Frequently Asked Questions (FAQ)

Post by yexiaobo » Thu Apr 07, 2016 6:34 pm

Wio Link FAQ

1. Power & Battery - Does Wio Link come with a Lipo battery?
Nope. Each Wio Link goes with a micro USB cable for charging or you can got a 3.7V Lipo battery locally. Here’s the specs for your kind reference - maximum input voltage: 4.2V; maximum charging current: 500mA

2. Power & Battery - Can I use a power adapter with Wio Link? Which type? And common battery holders?
There are two ways to power the Wio Link, Micro USB cable or a 3.7V Lipo battery. If both Micro USB and battery are plugged into the board, the battery will be charged by the USB power. You can use all kinds of power adapter which got Micro USB cable and 5Vdc output. The battery holder is a JST-2.0 connector.

3. Power Consumption - What’s the power consumption of Wio Link?
The average power consumption is 70mA. With a battery of 700mAh, it can keep alive up to 10 hours. There are Low-Power-APIs which allows you to change the Wio Link from working-mode to sleeping-mode. It will reduce average power consumption to 150uA or less.

4. Grove Cables - Are the Groves equipped with cables in all kits?
Yes, we have each Grove modules packed with one standard 4-pin Grove cable.

5. RESTful APIs - Where are the endpoints? The calls aren't required to go through some cloud servers are they? Is it an internet connection required or can they be made all through a local network?
We deploy the REST API server to iot.seeed.cc, so you can get access to sensor and actuator from iot.seeed.cc. At the moment, Wio Link must connect to the Internet. Also, we will open-source the server so as to enable users deploy local servers in very simple Docker way. With local servers deployed, they can utilize the compiling and data exchange service locally instead of going online.

6. Programming Methods Supported - Will other programming methods be supported, such as Arduino IDE?
Wio Link can be programed with Arduino IDE, in that case it will lose the functionality of RESTful APIs except you implement another one in the same time. Wio Link is mostly expected to archive the Web of Things conversion for physical hardwares, so interactions are expected to perform in web / internet. But no worries, the software architecture is flexible, you can pull down the source code to local and connect Wio Link to the local servers, then you could modify the source code which will be compiled.
If you would like to interact with Arduino or RPI, you can develop a 3rd-party module driver and here’s the guide: https://github.com/Seeed-Studio/Wio_Lin ... io-Link%3F and example driver: https://github.com/Seeed-Studio/Wio_Lin ... ve_example

7. Platform Supported -Does Wio Link support Windows Platform?
By now Wio Link provides Android and iOS two mobile Apps. We have all services as RESTful API, such like user accounts and OTA, following API documents, the third-party developers can build their own applications say Mobile Apps or Desktop Apps.
Wio Link is an community friendly project. It won't be limited to a certain platform. We really expect people can play with Wio Link in their way.

8. Can I use Wio Link to interact with existing systems?
Yes. Who Link can interact with your existing system in several ways. First, connect any GPIO of Wio Link to other system, select “Generic Digital Input” or “Generic Digital Output” virtual Grove modules in the mobile App, then send/read signals to/from the existing system with RESTful API calls. Second, connect the analog port of Wio Link to other system, select “Generic Analog Input” virtual Grove module in the mobile App, then read analog measurement for some physical quantity of your existing system. Third, to interact with existing system more flexible, you can develop a 3rd party module driver in which dispatch the requests from internet to your existing system through I2C or UART interface. We have a guide[1] about how to develop 3rd party module driver and also we can provide technical support for your development.
[1]https://github.com/Seeed-Studio/Wio_Lin ... r-wio-link


9. Is there any detailed documentation about Wio Link?
Yes. We have wiki pages for Wio Link. Please have a look at https://github.com/Seeed-Studio/Wio_Link/wiki. These wiki pages are more related to technology, for first getting started, please have a look at https://iot.seeed.cc.

10. How many Groves supported on Wio Link?
There are 150+ kinds of plug and play Groves modules available, among which 36 were supported on Wio Link till now, and you can find most of them in the Rewards, we're working to add more continuously.
Here's the list of supported Groves so far:
Grove - Moisture Sensor:
http://seeedstudio.com/wiki/Grove_-_Moisture_Sensor
Grove - Air quality sensor v1.3:
http://www.seeedstudio.com/wiki/Grove_- ... ensor_v1.3
Grove - Relay:
http://www.seeedstudio.com/wiki/Grove_-_Relay
Grove - SPDT Relay(30A):
http://www.seeedstudio.com/wiki/Grove_-_SPDT_Relay(30A)
Grove - Dry-Reed Relay:
http://www.seeedstudio.com/wiki/Grove_-_Dry-Reed_Relay
Grove - Solid State Relay:
http://www.seeedstudio.com/wiki/Grove_- ... tate_Relay
Grove - Button:
http://www.seeedstudio.com/wiki/Grove_-_Button
Grove - Button(P):
http://www.seeedstudio.com/wiki/Grove_-_Button
Grove - Digital Light Sensor:
http://www.seeedstudio.com/wiki/Grove_- ... ght_Sensor
Grove - Magnetic Switch:
http://www.seeedstudio.com/wiki/index.php
Grove - Barometer Sensor(BMP180):
http://www.seeedstudio.com/wiki/Grove_- ... r_(BMP180)
Grove - Multichannel Gas Sensor:
http://www.seeedstudio.com/wiki/Grove_- ... Gas_Sensor
Grove - Speaker:
http://www.seeedstudio.com/wiki/Grove_-_Speaker
Grove - EL Driver:
http://www.seeedstudio.com/wiki/Grove_-_EL_Driver
Grove - Rotary Angle Sensor(P):
http://www.seeedstudio.com/wiki/Grove_- ... gle_Sensor
Grove - Rotary Angle Sensor:
http://www.seeedstudio.com/wiki/Grove_- ... gle_Sensor
Grove - Gesture:
http://www.seeedstudio.com/wiki/Grove_-_Gesture_v1.0
Grove - 3-Axis Digital Accelerometer(±1.5g):
http://www.seeedstudio.com/wiki/Grove_- ... ter(±1.5g)
Grove - 3-Axis Digital Compass:
http://www.seeedstudio.com/wiki/Grove_- ... mpass_V1.0
Grove - 3-Axis Digital Gyro:
http://www.seeedstudio.com/wiki/Grove_- ... gital_Gyro
Grove - Temp&Humi Sensor:
http://www.seeedstudio.com/wiki/Grove-_ ... ity_Sensor
Grove - Temperature&Humidity Sensor Pro:
http://www.seeedstudio.com/wiki/Grove_- ... Sensor_Pro
Grove - Servo:
http://www.seeedstudio.com/wiki/Grove_-_Servo
Grove - IR Distance Interrupter:
http://www.seeedstudio.com/wiki/Grove_- ... _Interrupt
Grove - WS2812 RGB LED:
http://www.seeedstudio.com/depot/Digita ... -1665.html
Grove LED Bar v2.0:
http://www.seeedstudio.com/wiki/Grove_-_LED_Bar
Grove - OLED Display 1.12":
http://www.seeedstudio.com/wiki/Grove_- ... lay_128*64
Grove - PIR Motion Sensor:
http://www.seeedstudio.com/wiki/index.php
Grove - Temperature Sensor:
http://www.seeedstudio.com/wiki/Grove_- ... ensor_V1.2
Grove - Electromagnet:
http://www.seeedstudio.com/wiki/Grove_-_Electromagnet
Grove - I2C Motor Driver:
http://www.seeedstudio.com/wiki/Grove_- ... river_V1.3
Grove - Protoshield:
http://www.seeedstudio.com/wiki/Grove_-_Protoshield
Grove - I2C Hub:
http://www.seeedstudio.com/wiki/index.php
Grove - Buzzer:
http://www.seeedstudio.com/wiki/Grove_-_Buzzer
Grove - Recorder:
http://www.seeedstudio.com/wiki/Grove_-_Recorder
Grove - Ultrasonic Ranger:
http://www.seeedstudio.com/wiki/Grove_- ... nic_Ranger

11. When can I receive my rewards?
We shipped all board rewards & kit rewards till the end of March as scheduled. The shipping will take around 2 weeks to arrive, vary from different countries. Please wait a while patiently. If you haven’t received your reward till April 15th, please let us know and we will check the tracking numbers for you individual. Thanks for your understanding.

chuck.untulis
Pre-kindergarten
Pre-kindergarten
Posts: 2
Joined: Fri Apr 08, 2016 9:21 am

Re: Wio Link FAQ

Post by chuck.untulis » Fri Apr 08, 2016 11:23 am

Pointing people to a cute video http colon slash slash iot dot seeed dot cc slash that plays too fast for people to see what is on the screen and what is pressed is not helpful. It is certainly not for beginners, because it gives no hints to what can go wrong and how to isolate the problem or where to find more information. It is more a PR piece instead of documentation.

I keep try the steps but the things do not pop up as in the video.

Your apparent spam hammer does not allow your own URL. Obviously no AI is involved.

yexiaobo
Pre-kindergarten
Pre-kindergarten
Posts: 46
Joined: Tue Dec 11, 2012 10:53 am

Re: Wio Link FAQ

Post by yexiaobo » Thu Apr 14, 2016 11:01 am

chuck.untulis wrote:Pointing people to a cute video http colon slash slash iot dot seeed dot cc slash that plays too fast for people to see what is on the screen and what is pressed is not helpful. It is certainly not for beginners, because it gives no hints to what can go wrong and how to isolate the problem or where to find more information. It is more a PR piece instead of documentation.

I keep try the steps but the things do not pop up as in the video.

Your apparent spam hammer does not allow your own URL. Obviously no AI is involved.
Thanks for your feedback.

We are re-make new video for our document. It will be include more details, such as Setup, LED Status, etc.

And new document in process. We are plan release it end of this month.

Dgalgozy
Pre-kindergarten
Pre-kindergarten
Posts: 1
Joined: Mon Apr 18, 2016 7:02 am

Re: Wio Link Frequently Asked Questions (FAQ)

Post by Dgalgozy » Mon Apr 18, 2016 7:03 am

I have not received my Kick Starter reward yet. Is there a tracking number?

Post Reply