How can I combine your experiments?

Any problem about ARDX kit, Grove - Starter Kit (Plus),etc, you can post here.

Moderators: violet, jessie

Post Reply
User avatar
Jacket Chen
Staff
Staff
Posts: 662
Joined: Thu Jun 21, 2012 4:25 pm
Are you a staff member of seeedstudio?: yes
Which products/projects are your favorite?: Seeeduino Shields
Location: China

How can I combine your experiments?

Post by Jacket Chen » Tue Apr 14, 2015 4:17 pm

I bought your ARDX starter kit for Arduino hoping it would help my daughter's science fair project. How can I combine your experiments? She wants to remotely control (RF) LEDs and a noisemaker (piezo I guess), but if the wireless control is too hard to do, wants a push button. So basically I want to combine CIRC-02 + CIRC-06 with a pushbutton. (We only need 5 LEDs not 8; CIRC-07 has two pushbuttons, can't it be just done with one?) We have tried combining the projects and code ourselves and nothing has worked. Can do the individual projects, just not the combination. HOW CAN WE COMBINE THEM?
Maybe you can have the following demo tested. However, i don't try it yet ~~ :lol:

Code: Select all

int speakerPin = 9;
const int buttonPin = 2;
int ledPins[] = {4,5,6,7,8};

int length = 15; // the number of notes
char notes[] = "ccggaagffeeddc "; // a space represents a rest
int beats[] = { 1, 1, 1, 1, 1, 1, 2, 1, 1, 1, 1, 1, 1, 2, 4 };
int tempo = 300;

int buttonState = 0;

void setup() {
  pinMode(speakerPin, OUTPUT);
  pinMode(buttonPin, INPUT);
  
  for(int i = 0; i < 5; i++){         //this is a loop and will repeat eight times
      pinMode(ledPins[i],OUTPUT); //we use this to set each LED pin to output
  }
}

void loop() {
  
  while(buttonState == HIGH) {
    oneAfterAnotherNoLoop(); 
  for (int i = 0; i < length; i++) {
    if (notes[i] == ' ') {
      delay(beats[i] * tempo); // rest
    } else {
      playNote(notes[i], beats[i] * tempo);
    }
    
    // pause between notes
    delay(tempo / 2); 
   }
  }
  if(buttonState == LOW)
  {digitalWrite(speakerPin, LOW);}
}

void oneAfterAnotherNoLoop(){
  int delayTime = 100; //the time (in milliseconds) to pause between LEDs
                       //make smaller for quicker switching and larger for slower
  digitalWrite(ledPins[0], HIGH);  //Turns on LED #0 (connected to pin 2 )
  delay(delayTime);                //waits delayTime milliseconds
  digitalWrite(ledPins[1], HIGH);  //Turns on LED #1 (connected to pin 3 )
  delay(delayTime);                //waits delayTime milliseconds
  digitalWrite(ledPins[2], HIGH);  //Turns on LED #2 (connected to pin 4 )
  delay(delayTime);                //waits delayTime milliseconds
  digitalWrite(ledPins[3], HIGH);  //Turns on LED #3 (connected to pin 5 )
  delay(delayTime);                //waits delayTime milliseconds
  digitalWrite(ledPins[4], HIGH);  //Turns on LED #4 (connected to pin 6 )
  delay(delayTime);                //waits delayTime milliseconds
  digitalWrite(ledPins[5], HIGH);  //Turns on LED #5 (connected to pin 7 )
  delay(delayTime);                //waits delayTime milliseconds
  digitalWrite(ledPins[6], HIGH);  //Turns on LED #6 (connected to pin 8 )
  delay(delayTime);                //waits delayTime milliseconds
  digitalWrite(ledPins[7], HIGH);  //Turns on LED #7 (connected to pin 9 )
  delay(delayTime);                //waits delayTime milliseconds  
 
//Turns Each LED Off
  digitalWrite(ledPins[7], LOW);  //Turns on LED #0 (connected to pin 2 )
  delay(delayTime);                //waits delayTime milliseconds
  digitalWrite(ledPins[6], LOW);  //Turns on LED #1 (connected to pin 3 )
  delay(delayTime);                //waits delayTime milliseconds
  digitalWrite(ledPins[5], LOW);  //Turns on LED #2 (connected to pin 4 )
  delay(delayTime);                //waits delayTime milliseconds
  digitalWrite(ledPins[4], LOW);  //Turns on LED #3 (connected to pin 5 )
  delay(delayTime);                //waits delayTime milliseconds
  digitalWrite(ledPins[3], LOW);  //Turns on LED #4 (connected to pin 6 )
  delay(delayTime);                //waits delayTime milliseconds
  digitalWrite(ledPins[2], LOW);  //Turns on LED #5 (connected to pin 7 )
  delay(delayTime);                //waits delayTime milliseconds
  digitalWrite(ledPins[1], LOW);  //Turns on LED #6 (connected to pin 8 )
  delay(delayTime);                //waits delayTime milliseconds
  digitalWrite(ledPins[0], LOW);  //Turns on LED #7 (connected to pin 9 )
  delay(delayTime);                //waits delayTime milliseconds  
}

void playTone(int tone, int duration) {
  for (long i = 0; i < duration * 1000L; i += tone * 2) {
    digitalWrite(speakerPin, HIGH);
    delayMicroseconds(tone);
    digitalWrite(speakerPin, LOW);
    delayMicroseconds(tone);
  }
}

void playNote(char note, int duration) {
  char names[] = { 'c', 'd', 'e', 'f', 'g', 'a', 'b', 'C' };
  int tones[] = { 1915, 1700, 1519, 1432, 1275, 1136, 1014, 956 };
  
  // play the tone corresponding to the note name
  for (int i = 0; i < 8; i++) {
    if (names[i] == note) {
      playTone(tones[i], duration);
    }
  }
}
Jacket
Love little, love long.

Post Reply