dimension of grove sensor o2 (holes)

Hello, i ordered a grove O2 sensor and im making a 3D printed housing for it. i was searching the web for the dimensions of the pcb. but couldnt find anything.

Can someone measure this for me?



Greetings

Hope this helps @Mathias_Vangompel



A= 40mm

B= 20mm

C= 30mm

D= 10mm



All dimensions are to the center of each hole

Hole dimension is 3mm



Note :- Each hole is on the edge of the board and the board can not lie flat, there is the connector terminal one side and circuits the other so it needs a stand off on each mount.



Please see additional photos for clarity.
IMG_20180722_101221_resized_20180722_101247236.jpg
IMG_20180722_101153_resized_20180722_101259931.jpg
IMG_20180722_101147_resized_20180722_101310341.jpg
Grove O2 board.jpg

hmmm… keeps removing the last attachment… this is the board with the sensor attached…
IMG_20180722_101553_resized_20180722_101604077.jpg

Hi, you also can download eagle board files from <LINK_TEXT text=“https://github.com/SeeedDocument/Grove_ … ics_O2.zip”>https://github.com/SeeedDocument/Grove_Gas_Sensor_O2/raw/master/resources/Schematics_O2.zip</LINK_TEXT>. then click Draw–> Dimension to measure the sizes. thanks.



Seeed techsupport team

Bill