Data sheets for Sidekick kit?

Hello,



I’m wondering if there are any data sheets available for the components in the sidekick kit.



Specifically I’m looking for a data sheet for the included buzzer for the rated frequency/voltage/current.



Thank you!

Hi there, please refer to <LINK_TEXT text=“http://wiki.seeedstudio.com/Sidekick_Ba … rduino_V2/”>http://wiki.seeedstudio.com/Sidekick_Basic_Kit_for_Arduino_V2/</LINK_TEXT>.



Here is the spec for buzzer.



1 Rated Voltage (VDC) 3

2 Operating Voltage (VDC) 1.5~5

3 Resonant Frequency (Hz) 2700±300

4 Sound Output at 10cm (dB) ≥85

5 Current Consumption (mA) ≤30

6 Operating Temperature (℃) -20~+70

7 Storage Temperature (℃) -30~+80



Seeed techsupport team

Bill