Labview on ReTerminal

Hi,

I have used LabView on Linux before but have only made it work on Fedora and Intel Atom platform (almost 10years ago on V8,5).
Has anyone successfully installed Fedora on ReTerminal, and if so can that someone point me to a HowTo somewhere?
OR…even better
Has anyone made LabView Runtime run on ReTerminal?

I have LabView Version 8.5 and 14.1 available and so i will need to install one of the two matching runtimes for me to have success.

Anyone out there with any experience on this?

Hello,

I came across this:

You could have a try.

Also, since the reTerminal is based on a RPi CM4, you could basically run most applications and operating systems which are supported by the Raspberry Pi 4.

Best Regards,
Lakshantha