How to use Grove W600 in IoT project

Hello, I’m very novice with Arduino, but for my first project, I would like to make a smart greenhouse. For that, I’m using different grove sensors, Arduino Uno and the base shield V.2… I have different sensors as the moisture sensor which is supposed to print on my display the value. I bought the W600 grove module to send those values on a Cloud like ThingSpeak, Dweet.io … I checked the W600 library but I only found some exemple to connect the module to internet, I don’t really know how to use it to send my data on the cloud.

I didn’t find many stuff on google concerning the use of W600 grove.
I would like to know how to use the W600 library to send my data on the cloud. Thank you for your answer!

I put the part of my code concerned, and the sta_mode_connect exemple of the library. This is the part of my code which is supposed to read the value of the moisture sensor:

const int moistureSensor = A0;

void setup() {
Serial.begin(9600);
pinMode(moistureSensor, INPUT);
}

void loop() {
int moistureRaw = analogRead(moistureSensor);
int moistureReal = map(moistureRaw, 950, 0, 0, 100); //950 is the max moisture value
Serial.print("Moisture of the plant : ");
Serial.println(moistureReal);
Serial.print(" % ");
delay(1000);
} 

And this is the exemple sta_mode_connect in the speed W600 library :

#include "seeed_w600.h"

// Architecture specific include
#if defined(ARDUINO_ARCH_AVR)
    #pragma message("Defined architecture for ARDUINO_ARCH_AVR.")
    SoftwareSerial softSerial(2, 3);
    #define SERIAL Serial

#elif defined(ARDUINO_ARCH_SAM)
    #pragma message("Defined architecture for ARDUINO_ARCH_SAM.")
    #define SERIAL SerialUSB

#elif defined(ARDUINO_ARCH_SAMD)
    #pragma message("Defined architecture for ARDUINO_ARCH_SAMD.")
    #define SERIAL SerialUSB

#elif defined(ARDUINO_ARCH_STM32F4)
    #pragma message("Defined architecture for ARDUINO_ARCH_STM32F4.")
    #define SERIAL SerialUSB
#else
    SoftwareSerial softSerial(2, 3);
    #define SERIAL Serial
#endif

#define debug  SERIAL


String msg;
AtWifi wifi;

String SSID = "STU-EE";
String PSWD = "stu-ee-2022";

void setup() {
    debug.begin(115200);
    #if defined(SAMD21)
    wifi.begin(Serial, 9600);
    #else
    wifi.begin(softSerial, 9600);
    #endif

    wifi.wifiReset();
    delay(1000);

    if (!wifi.wifiSetMode(STA)) {
        debug.println("Set config mode failed!");
        return ;
    }
    delay(100);
    if (!wifi.wifiStaSetTargetApSsid(SSID)) {
        debug.println("Set target AP ssid failed!!");
        return;
    }
    delay(100);
    if (!wifi.wifiStaSetTargetApPswd(PSWD)) {
        debug.println("Set target AP password failed!!");
        return;
    }
    delay(100);

    if (!wifi.joinNetwork()) {
        debug.println("Join to AP network failed!!");
        return;
    }

    debug.println("Connect to target wifi : ");
    debug.print("Target AP SSID = ");
    debug.println(SSID);
    debug.print("Target AP PSWD = ");
    debug.println(PSWD);
    debug.println("OK!");
}


void loop() {
    delay(1000);
    if (wifi.getWifiConnectStatus(msg)) {
        debug.println("My IP = [status],[ip],[netmask],[gateway],[dns] : ");
        debug.println(msg);
        while (1);
    }

}

In general, IoT cloud manufacturers will provide the appropriate SDK. this SDK directly calls the network interface, do you need the appropriate SDK for the connected iot cloud?
eg:

HI
Does AWS IOT support W600 or any library?
Thank you
G Cohen

Hi and sorry for the up. Are there any analogs for W600 module exists?
Thanks in advance
Frank